- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Create a variable
Create a variable for an object or variable in the folder in
Project
view
. The new variable displays values specified in Properties
at runtime. - InProject view, select the folder to contain the variable.
- In the view toolbar, selectAddnewand then selectAll > Model.
- Select the variable type:
- Variable
- AnalogVariable
- Nodepointer
- (optional) To display and select a different data type, selectShow alland then select the data type.
The new variable appears in
Properties
.Provide Feedback