- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Configure Alarm widgets
After you add Alarm manager and Alarm summary to your project, you need to configure the
widgets.
- InProject ViewunlockAlarmManager (type)and adjust widget layout, model, and logic.
- In, for any alarm filters that you want accessible for the widgets, selectTrue.
- In 2 that you want active, select, for any alarms enabled inTrue.
- (Optional) InProject ViewUnlockAlarmSummary (type)and adjust widget layout, model, and logic.
- In, for any alarm filters that you want accessible for the widgets, selectTrue.
- In 5 that you want active, select, for any alarms enabled inTrue.
- InProject Viewselect and:
- InAlarmWidgetsFilters (type)adjust the filters window parameters.
- InAlarmWidgetsTimedShelve (type)adjust the max time shelve duration and preset time shelve duration.
- InAlarmWidgetsViewDetail (type)adjust the information that displays in the Alarm Details view at runtime.TIP:Alarm Detailsview by default displays all avaqilable Alarm information. You can remove elements from this view, if you do not require them. For example, if you do not want the Details view to display tags, inProjectview you can select all Tags underAlarmDetailsand delete them.
- InAlarmSummaryButton (type), adjust the properties of all Alarm Summary widget buttons.
- InAlarmManagerButton (type), adjust the properties of all Alarm Manager widget buttons.
For all Alarm Widget Components, you can also adjust the layout. For example, you can modify button names, placement, sizes and background colors.
Provide Feedback