- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Conditional converter
Verify if the source variable value is
True
or False
.Properties
Property | Description |
---|---|
True value | The value of the expression that is True . |
False value | The value of the expression that is False . |
Mode | The direction of the dynamic link:
|
Source
The condition variable (Boolean).
Output
A
True
or False
value.Example
In the following example, the conditional converter:
- Sets the text color of a label to green if a switch is selected.
- Sets the text color of a label to red if a switch is cleared.

conditional converter
Provide Feedback