- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Animation properties
Configure animations by editing animation properties.
TIP:
For animation examples, download, extract, and open the
project from AnimationsExample.zip.
Number animation
A simple animation based on a variable value change over specific time.
Property | Description |
---|---|
From | Start value of the range |
To | End value of the range |
Duration | Duration of the animation in milliseconds |
Interpolation | The type of interpolation when animation value changes |
Target | Target node of the animation |
Running | Boolean value |
Loops | Number of consecutive animation playbacks. The -1 value sets continuous animation playback. |
Sequential animation
Groups of animation executed in a sequential order.
Property | Description |
---|---|
Running | Boolean value |
Loops | Number of consecutive animation playbacks. The -1 value sets continuous animation playback. |
Parallel animation
Groups of animation executed in a parallel order.
Property | Description |
---|---|
Running | Boolean value |
Loops | Number of consecutive animation playbacks. The -1 value sets continuous animation playback. |
animation
Provide Feedback