- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Zoom in and zoom out a trend chart
Zoom the X and Y axes of a trend chart to focus on specific data. Zoom in and out the trend chart axes together or separately. Zooming applies only to the
Normal
and Time range
trend modes.- To zoom the trend chart:
- Use the pinch-to-zoom gesture.
- Place the mouse pointer in the area of interest of the trend chart and scroll forward or backward.
- Select the trend chart and select+or-.
- To zoom the X-axis only, place the mouse pointer anywhere in the trend chart, hold, and then scroll up or down.Ctrl
- To zoom the Y-axis only, place the mouse pointer anywhere in the trend chart, hold, and then scroll up or down.Alt
zoom
Provide Feedback