- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Configure TLS without client certificate
The following are required:
- A Certificate Authority (CA) certificate of the CA that has signed the Broker certificate.
- CA certificated Broker certificate.
- Server Private key for decryption.
- OpenSSL installed on the device.
TIP:
Do not use encryption for the server certificate when generating keys (the
-des3
switch). This creates a password protected key which the
broker is unable to decode.- In Command Prompt, create a CA key pair by entering:openssl genrsa -des3 -out ca.key 2048
- Create CA certificate and use the CA key from 1 to sign it:openssl req -new -x509 -days 1826 -key ca.key -out ca.crt
- Create a broker key pair without password protection:openssl genrsa -out server.key 2048
- Create a broker certificate request using key from 3:openssl req -new -out server.csr -key server.key
- Use the CA certificate to sign the broker certificate request from 4:openssl x509 -req -in server.csr -CA ca.crt -CAkey ca.key -CAcreateserial -out server.crt -days 360
- Place all files in a single directory on the MQTT broker.
- Copy the CA certificate file to the MQTT client.
- Edit theFactoryTalk Optixclient security properties to use the CA certificate.
tls
certificate
Provide Feedback