Configure OPC UA server certificates and keys

Configure OPC UA server certificates and keys

Edit the properties of an OPC UA server to configure the public certificates and private keys.
Prerequisites
  1. To configure OPC UA server certificates and keys
  2. In
    Project view
    , select an
    OPCUAServer
    object.
  3. In
    Properties
    , next to
    Server certificate file
    , select
    Browse
    .
  4. In :
    • If the certificate is listed, select the certificate and choose
      Select
      .
    • If the certificate is not listed:
      1. Select
        Import file(s)
        .
      2. Select the certificate. For more information, see Certificates and keys location.
      3. Choose
        Select
        .
  5. Next to
    Server private key
    , select
    Browse
    .
  6. In :
    • If the private key is listed, select the private key and choose
      Select
      .
    • If the private key is not listed:
      1. Select
        Import file(s)
        .
      2. Select the private key. For more information, see Certificates and keys location.
      3. Choose
        Select
        .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.