- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Project nodes
Use
Project view
to create and manage nodes and folders in your project.Project view
Project view
displays a tree structure comprised of nodes. The nodes are objects and variables organized in folders. Each folder has a dedicated icon and context menu. The context menu displays objects that you can create in that folder. Any subfolder that you create displays the same options as the folder on which it is based. You can create multiple versions of a folder.
TIP:
Search
Project view
to find contents without having to navigate and expand folders. Split Project view
to see multiple areas of the project simultaneously. For more information about the
Project view
pane, see Project view.Node types
Project nodes include different object types, object instances, and variables. For more information on how to create, delete, rename, and manage different node kinds, see:
project view
Provide Feedback