- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Export a project
Export a project to archive the project or to send the project to another user in a single file. You can protect the exported project with a password.
- In the main toolbar, select the drop down next to.Save
- Select.
- (optional) Change the project name.
- (optional) Change the location to export the project.
- (optional) Enter a password to protect the exported project.
- SelectExport.
The project is exported to the indicated location and is
appended with the extension .optixz.
Provide Feedback