Recipes editor

Recipes editor

The recipes editor widget contains the graphical objects and NetLogics required to display and manage the recipes at runtime.
Use the recipes editor widget to:
  • Display ingredients and values of a stored recipe during editing or loading the controller
  • Create, edit, or delete a recipe
  • Store a recipe in the database
  • Load a recipe from the
    FactoryTalk Optix Application
    to the controller
  • Load a recipe from the controller to the
    FactoryTalk Optix Application

Interface

Recipes editor interface
Recipes editor items
Item
Name
Description
1
Recipe name
Assign a name to a new recipe or select an existing recipe.
2
Recipe control buttons
  • Save
    . Store the recipe in the database during editing.
  • Delete
    . Delete the selected recipe from the database.
  • Load
    . Load the recipe values from the controller to the
    FTOptixApplication
    .
  • Apply
    . Apply the selected recipe on the controller.
3
Ingredients list
Recipe schema ingredients.
4
Ingredient values editor
Editable values of the recipe ingredients.
5
Applied ingredient values
Values of the ingredients on the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal