Apply a stylesheet to a report

Apply a stylesheet to a report

Use the
StyleSheet
property to specify an instance of the selected style to apply to the report.
The units of measurement in reports are specified in
FactoryTalk Optix Studio
options. See Set options. The language that you select for a project determines the default unit of measurement. For example, if you set the language option to
en-US
,
FactoryTalk Optix Studio
uses inches as the default unit of measurement for reports.
  1. In
    Project
    view
    , select your
    Report#
    object.
  2. In
    Properties
    , in
    StyleSheet
    , select the drop-down arrow to select the stylesheet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal