- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Idle timeout configuration
Configure a timeout when there is a lack of user activity in the
FactoryTalk Optix
. A timeout can trigger any custom event.
TIP:
To configure a timeout, the application must have interactive graphic objects. At runtime, inactivity includes a lack of cursor movements, keyboard actions, and user interactions. You can configure an idle timeout for either a specific page or an entire session.
Provide Feedback