View committed changes

View committed changes

View the committed changes of the open project by viewing the project history.
  1. In the toolbar, select
    View history
    .
  2. In
    Version history
    , select a commit.
    TIP:
    Local history
    represents a change that is committed to the local repository and
    Remote history
    represents a change that is pushed to the remote repository.
    The changes in the commit appear highlighted.
  3. Expand a highlighted object to view the changes in the object.
    TIP: Values that change in an object are crossed out and an arrow points to the new value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal