Deploying projects

Deploying projects

Compile projects to
FactoryTalk Optix Applications
and then deploy the applications to target devices.
To determine which presentation engine is required for the mode in which
FactoryTalk Optix
will be running, see FactoryTalk Optix runtime modes.
You can manage the target devices to which you deploy
FactoryTalk Optix Applications
. See Manage target devices and Deploy a FactoryTalk Optix Application.
For target devices not accessible in the network, you can export
FactoryTalk Optix Applications
from
FactoryTalk Optix Studio
and then import them to target devices. See Export a FactoryTalk Optix Application and Import a FactoryTalk Optix Application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal