- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
LogicObject.GetAlias(string)
Returns an
IUANode
C# object that corresponds to the node pointed to by the alias passed in the argument. Access the node to which a known alias pointsstatic IUANode GetAlias(stringaliasName);
Arguments
- aliasName(string)
- TheBrowseNameof the alias.
Returns
- IUANode
- A C# object that corresponds to the node pointed to by the alias.
Example
The following example shows an API that returns a C# object corresponding to the node pointed to by the alias
Motor
, which Speed
property value is read and assigned to the myMotorSpeed
variable.
TIP:
The
(MotorType)
cast operator changes the object type returned by the API from IUANode
to MotorType
. This is useful if you want to access the Speed
property of refMotor
directly.var refMotor = (MotorType)LogicObject.GetAlias("Motor"); var myMotorSpeed = refMotor.Speed;
Provide Feedback