- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
NuGet packages
Some library widgets and scripts require specific NuGet packages to be installed.
For more information about NuGet, see What is NuGet and what does it do? | Microsoft Docs.
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 8 destination
framework. To debug FactoryTalk Optix Applications
with Visual Studio®
or Visual Studio Code®
, install .NET SDK.
IMPORTANT:
Rockwell Automation
is not responsible for any third-party software, including but not limited to its
performance, security, updates, or compatibility with our products. Any use of third-party
software is at your own risk, and we do not provide support, warranties, or guarantees for
such software. Users should refer to the respective third-party providers for assistance and
licensing terms.Install NuGet packages in the code editor of your choice. See Install NuGet packages in Visual Studio and Install NuGet packages in Visual Studio Code.
nuget
Provide Feedback