Start debugging on the remote machine

Start debugging on the remote machine

Deploy the runtime application to the remote machine and start the debugging process on the development machine.
  1. To start debugging on the remote machine
  2. From the main toolbar, select
    Open .NET Solution
    .
    The default external code editor opens.
    TIP: Rockwell Automation recommends using
    Visual Studio®
    2022 or
    Visual Studio Code
    as the default code editor. Some development assistance features may not be available when using a different code editor.
  3. From
    FactoryTalk Optix Studio
    , deploy the
    FTOptixApplication
    to the target device.
    For more information, see Deploy a FactoryTalk Optix Application.
  4. In
    Visual Studio
    , configure and start the debugging process.
    Attach to process with these settings:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.