- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Open the project in an external code editor
You can open the entire project in an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
- To open the project in an external code editor
- From the main toolbar, selectOpen .NET Solution.The default external code editor opens.TIP: Rockwell Automation recommends usingVisual Studio®2022 orVisual Studio Codeas the default code editor. Some development assistance features may not be available when using a different code editor.
Provide Feedback