An object is an element that identifies a physical object such as a motor or a non-physical object such as a digital alarm.
Object components
An object can contain:
Display name
Description
Variables
Nested objects
Object example
A physical motor is a mechanical object with specific operational characteristics such as
acceleration, speed, and torque. The Motor object in the project is an object that contains
the same properties.