- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Main toolbar
The main toolbar at the top of
FactoryTalk Optix Studio
contains buttons used by all views in the software.Item | Description | Function |
---|---|---|
![]() | Project | Opens the Start page. The Start page allows you to create, open, or close a project. |
Save | Saves the project. Select an option from the list to:
| |
![]() | Save and Commit | Saves changes and commit the changes to back them up in the local repository. |
Push to remote | Pushes saved and committed changes to the remote repository for users to see the latest changes to the project. | |
Pull from remote | Pulls the latest changes from the remote repository to see the latest changes that other users have made. | |
![]() | View History | Views the history of changes to the project. Restore any commit to revert to a previous version of the project. |
Undo | Cancels the last operation. | |
Redo | Repeats the last operation. | |
![]() | Search in project |
Search for specific object names or values in a project to quickly find objects. |
Browse project files | Opens the project resource window for displaying, importing, or deleting project files such as images, videos, documents, and certificates. | |
Template Libraries | Opens the default and custom libraries and template variables. | |
![]() | Open .NET Solution | Opens the .NET project to incorporate additional functionality using custom C# code. |
Open dashboard page | Opens a configuration dashboard to begin designing your user interface. Select the list to configure the connected device, data logging, and recipes, or manage users and groups. | |
![]() | Stop | Stops the application that is running on the target device. |
Run on Emulator | Compiles, transfers, and runs the application on the selected target device or emulator. Select a different target device from the list. | |
![]() | VPN | Opens a VPN connection. |
![]() | Remote Desktop | Opens a Remote Desktop connection. |
Provide Feedback