- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Properties pane
Use the
Properties
pane to display variables for the selected object. Property values change the appearance and display of that object at runtime.Properties pane columns

Item | Name | Description |
---|---|---|
![]() | Property name column | Navigate through the properties available for a selected object. Select any property and start typing the name of the property to find. |
![]() | Property value column | Edit property values. To edit the values of some properties quickly, select the value and start typing. The values may automatically complete as you type. |
TIP:
You can navigate through properties and values by selecting them with your mouse or by using the arrow keyboard keys.
Properties pane buttons
Item | Function |
---|---|
![]() Group by category | Organize the properties by category. |
![]() Sort alphabetically | Sort the properties in alphabetical order. |
![]() Add new | Add a property to the node. Add a display name, variable, alias, or audit signature. In the Events category of the Properties pane, this button adds an event from the Events header or a new method for the selected event. |
Delete | Remove an added property from the Properties pane or reset the value of a default property.Delete the selected method in Events . Deleting all methods from an added event deletes the event. |
![]() Detach view | Detach the pane from the main window. |
![]() Attach view | Detach the pane to the main window. |
![]() Open with editor | Open the editor for the selected object. This button is valid for only certain object types. |
Property pane context menus
To open the property context menu, right-click the property name.
Item | Description |
---|---|
New | Create child properties, variables, and aliases, or to create events based on the selected property. |
Delete | Delete properties, variables, and aliases. |
Copy | Copy child properties, variables, and aliases. |
Paste | Paste child properties, variables, and aliases. |
Collapse all | Collapse all children nodes of properties, variables, and aliases. |
Show References | Display which objects or variables reference the property. |
Copy path to node | Copy the path of properties, variables, and aliases in the project. |
Change modelling rule | Set the modelling rule:
|
Model analysis | Visualize the project information model in the form of a graph. See Display information model graphs. |
To open the property value context menu, right-click the property value.
Item | Description |
---|---|
Copy | Copy the selected property value. |
Paste | Paste the copied property value to the selected property value. |
Reset Value | Reset the property value to the default value. |
Provide Feedback