Develop a motor management dashboard

Develop a motor management dashboard

The UI contains a list of motors and gauges that display speed and acceleration values.
Application example
NOTE:
Download a sample project:
MotorManagementDashboard.zip
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.