Develop an archives manager
Use the preconfigured Zip Unzip NetLogic to create, extract, and password-protect ZIP archives.
Example application
![](/content/dam/dita/en/factorytalk-optix/current/_images/archives-manager.png/_jcr_content/renditions/original)
TIP:
You can download a sample project from:
ArchivesManager.zipPrerequisites
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback