- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a retentivity storage
Add persistence to user settings.
- InProject view, right-clickRetentivityand select .
- InProperties, next toNodes, select.
- Create a dynamic link betweenNode1and .For more information about dynamic links, see Create dynamic links.
Provide Feedback