Create elements for controlling the min value

Create elements for controlling the min value

Create a label and a gauge to control the minimum value.
  1. Create the minimum value label:
    1. In
      Project view
      , right-click
      MainWindow (Type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      MinValueLabel
      .
    3. In
      Properties
      and set
      Text
      to
      Minimum Value
      .
  2. Create the min gauge:
    1. In
      Project view
      , right-click
      MainWindow (Type)
      and select
      New
      Base controls
      Linear gauge
      .
    2. Hover-over the gauge, select
      Edit
      , and enter
      MinGauge
      .
    3. In
      Properties
      , create a dynamic link between
      Value
      and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      Low limit
      .
      For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.