- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Animate the side menu
- Select the side menu shape, and inPropertiesselect, and selectVariable.
- Rename the new variable toSideMenuActive
- Change the variable data type to Boolean.
- Select the button, and inEvents, next toMouseClick Event:
- Select.
- Select.
- ChooseSelect.
- InEvents, next toVariableToModifyselect.Add Dynamic Link
- Select.
- Select the side menu, and inPropertiesnext toLeft marginselect.Add Dynamic Link
- In theAdvancedtab, next toLeft margin:
- Select.
- SelectConditional converter.
- SetFalse valueto-140
- Next toCondition Dynamic linkselect.Add Dynamic Link
- Select.
- SelectOK.
Provide Feedback