- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a side menu
- InProject view, right-clickMainWindow (type)and select .
- (optional) Adjust the rectangle size as needed.
- (optional) Rename the shape accordingly.
- InProperties:
- Set aFill color.
- SetLeft marginto-140
- InProject view, right-clickMainWindow (type)and select .
Provide Feedback