- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a vertical layout
Defining vertical layout is necessary to distribute automatically generated graphical elements in an expected way.
- Right-clickMainWindow (type)and select .
- InProperties, setHorizontal alignmenttoRight.
- SetVertical alignmenttoStretch.
Provide Feedback