Faceplate Control - General

Faceplate Control - General

Use this tab to define/modify how the control operates.
Parameters
Communication
Select
RSLinx Classic
OPC Server or
FactoryTalk Linx
. If you select
RSLinx Classic
OPC Server, you must also specify:
  • whether to launch remotely
    • the access path to the remote machine
If you select
FactoryTalk Linx
FactoryTalk
, you must also specify the
FactoryTalk
Area
Tag
Enter the name of a specific function block instruction to connect with this control.
Update Rate
Enter the Update Rate of the control in seconds. You can click the arrows to increment this value in 0.25 second increments. The default value is 1.00 second.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.