- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Character string literals
Character string literals include single byte or double byte encoded characters. A single-byte string literal is a sequence of zero or more characters that are prefixed and terminated by the single quote character ('). In single byte character strings, the three-character combination of the dollar sign ($) followed by two hexadecimal digits is interpreted as the hexadecimal representation of the eight-bit character code as shown in the following table.
TIP:
Character string literals are only applicable to the CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers. Studio 5000 only supports single byte characters.
Character string literals
No. | Description | Example |
1a | Empty string (length zero) | '' |
1b | String of length one or character CHAR containing a single character | 'A' |
1c | String of length one or character CHAR containing the “space” character | ' ' |
1d | String of length one or character CHAR containing the “single quote” character | '$'' |
1e | String of length one or character CHAR containing the “double quote” character | '"' |
1f | Support of two character combinations | '$R$L' |
1g | Support of a character representation with ‘$’ and two hexadecimal characters | '$0A' |
Two-character combinations in character strings
No. | Description | Example |
1 | Dollar sign | $$ |
2 | Single quote | $' |
3 | Line feed | $L or $I |
4 | Newline | $N or $n |
5 | Form feed (page) | $P or $p |
6 | Carriage return | $R or $r |
7 | Tabulator | $T or $t |
TIP:
The newline character provides an implementation-independent means of defining the end of a line of data for both physical and file I/O; for printing, the effect is that of ending a line of data and resuming printing at the beginning of the next line.
The $' combination is only valid inside single quoted string literals.
Integer literal suffixes
This table lists suffixes you can add to integer literals in Structured Text, and the corresponding range for each suffix.
Suffix | Literal data type | Range |
---|---|---|
None | DINT | -2,147,483,648 to 2,147,483,648 |
L | LINT | -9,223,372,036,854,775,808 to 9,223,372,036,854,775,808 |
U | UDINT | 0 to 4,294,967,295 |
UL | ULINT | 0 to 18,446,744,073,709,551,615 |
Provide Feedback