Attach High Reference Signals - Input - FLEX I/O Calibration

Attach High Reference Signals - Input - FLEX I/O Calibration

To attach high reference signals for gain calibration:
gain
The ratio of the magnitude of the output signal with respect to that of the input signal.
In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
  1. Set the precision voltage/current source to the correct value.
  2. Select
    Next
    to perform gain calibration.
The module reads the signal and calibrates.
You may also select:
  • Retry
    if an error occurs and you need to repeat a step in the calibration process.
    TIP:
    This button is only enabled when an error occurs.
  • Stop
    to cancel calibration and exit the calibration.
  • Help
    for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal