- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Connected to Upload dialog box - Options tab
This dialog box indicates whether the project file matches the project in the controller, and provides information about the correlation status of the project file. Also use this dialog box for limited access to controller status information and to browse for a specific project file from this dialog box.
Parameters
Condition
Describes the correlation status of the open project.
Refer to
Correlate a project with a controller
for a list of all possible conditions.Connected Controller:
- Controller NameThe name of the controller to which the software is connected.
- Controller TypeThe controller type to which the software is connected.
- Comm PathThe communications path being used to connect to the controller.
- Serial NumberThe serial number of the Safety controller. This option is enabled for Safety controllers only.
- SecurityThe Security Authority bound to the controller. Refer to theController Propertiesdialog box,Securitytab to configure a Security Authority for a controller.
Offline Project:
- Controller NameThe name of the controller in the offline project file.
- Controller TypeThe controller type in the offline project file.
- FileThe name of the project file, including its full path. This field is blank if no project was open to start with, and a project file with the name found in the controller was not found in the project directory.
- Serial NumberThe serial number of the Safety controller associated with the Safety application. This option is enabled for Safety controllers only.
- SecurityThe Security Authority assigned for the controller used in the offline project.
Prohibit online edits during upload
Select this check box to prevent online edits in other instances of the project during project upload.
Upload
Select this button to start the Upload function to upload the connected controller into the open project file. When selected, you are prompted to save any changes made in the open file. When the upload occurs, documentation associated with objects in the controller is preserved; unused comments and descriptions are deleted.
If the upload is successful, the system goes online. If the upload fails, errors are listed in the Output window.
Download
Select this button to start the download process. If the download is successful, the application goes online. If the download is unsuccessful, an error appears, and the application returns to the offline state.
In either case, the dialog box closes.
Select File
Select this button to access the
Select File
dialog box to choose a different project file. Choose an existing file, or enter the name of a new file for the system to create and upload into.See alsoProvide Feedback