Go Online Using Recent Communications Path dialog box
Use this dialog box to go online using a recent communications path. It is similar to the
Select Recent Communications Path
dialog box, except that instead of simply using it to choose a path, the Logix Designer
application also attempts to go online using that path.Parameters
Controller
Select the controller with which to go online.
Path
Select the communications path with which to go online.
Go Online
Select to go online using the selected recent communications path.
Provide Feedback