Select File dialog box

Select File dialog box

Use this dialog box to select the project file into which to upload.
When this dialog box appears and no project is open,
File Name
defaults to the name of the connected controller. Otherwise, the field contains the name of the open project.
Create a new or select an existing file from this dialog box. Creating a new file creates and uploads a new project file. If choosing an existing file that is correlated with the online image, the project goes online, as reflected in the status bar. If choosing an existing file that is not correlated, the
Connected
dialog box opens.
Parameters
Look in:
Select the directory in which to look for the project file.
Up One Level
Select to go up one level in the directory tree.
Create New Folder
Select to create a new folder in the current directory.
List
Select to display a list of files in this directory.
Details
Select to display a list of files in this directory with all of the associated file details (for example, file size, date).
File name:
Enter the name of the file into which to upload.
Files of type:
Choose the type of file to search. In the
Logix Designer
application, this is a file with the ACD extension.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal