Use floating tool windows

Use floating tool windows

You can float a Floating window Tool Window to place it at any location on top of the
Logix Designer
application main and other windows.
Floating tool window restrictions:
  • You can only float a docked tool window.
  • You cannot float an auto hide tool window.
You can size a floating window. Position the mouse pointer on any window border until the pointer becomes a two-headed arrow. Press and hold the mouse button and drag the double-headed arrow to resize the window. When the window is the desired size, release the mouse button.
To float a Tool Window:
  1. In the Tool Window's title bar, click dropping locator down sign selected
    (Window State)
    and select
    Float
    . You can also double-click or drag the window's title bar.
    TIP:
    A floating Tool Window has only a Close button in its title bar. To display a floating Tool Window's options, right-click the floating window's toolbar.
  2. To position a floating Tool window, drag and drop it as desired. For more information, see Use Drag and Drop Functionality.
  3. To make the Tool Window stationary again, see Use docked tool windows.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.