Create-Configure Module Logix Block Fieldbus Logix Function Block
Use this tab to create/view module properties for the Logix Block Fieldbus Logix function block. In order to use this module, the parent module must be a 1757-FFLD or 1757-FFPC module.
Note that the first three parameters on this tab are read-only. These parameters provide you with information on:
- The type and description of the module being created.
- The vendor of the module being created.
- The name of the parent module.
To create a module
- InName, enter the name to use for this module.Use an IEC 61131-3 name. This field is required. If incomplete, an error message appears when exiting this tab. An error message also appears if a duplicate name is detected or an invalid character entered. If the maximum allowable name length is exceeded, the software ignores the extra character(s).
- InDescription, enter a description for the module (optional), up to 128 characters.Use any printable character in this field. If the maximum length is exceeded, the software ignores any extra character(s).
- From theComm Formatlist, choose the communication format used between the module and the controller.When choosing a communication format, the configuration formats for the module are also defined. For the 1757-FFPC module, choose from Data and Listen Only.TIP: Once you create a module, you cannot change the communication format. To change configuration, you must delete and recreate the module.
- Choose the minor revision number of your module.The revision is divided into the major revision and minor revision. The major revision displays statically on this dialog; edit this value from theSelect Module Typedialog.The major revision indicates the revision of the interface to the module. Valid values are in the range from 0 to 127. The minor revision indicates the firmware revision. Valid values are in the range from 0 to 255, with 1 being the default value.
- From the Electronic Keying list, choose Compatible Module, Exact Match, or Disable Keying.
- View status information if you wish.
Provide Feedback