- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Viewing and Printing the Instruction Signature
When the instruction signature has been generated, the Logix Designer application displays the instruction with the blue seal icon in the Controller Organizer, on the Add-On Instruction title bar, and in the Logic Editor.

When an instruction is sealed, the instruction signature is displayed on the faceplate of the instruction in the Ladder Diagram Editor and the Function Block Diagram Editor.


You can turn on or off the display of the instruction signature in the Workstation Options dialog box of the Logix Designer application. To access the Workstation Options dialog box, choose Options from the Tools menu.
You can also view the instruction signature and the safety instruction signature on the Quick View pane of the Controller Organizer and on the Signature tab of the Instruction Definition Editor dialog box.
The Add-On Instruction name, revision, instruction signature, safety instruction signature, and timestamp are printed on the Add-On Instruction Signature Listing report. You can also choose to include the instruction signature, safety instruction signature, and signature history on the Add-On Instruction Definition report by clicking Print Options on the Generate Report dialog box.
Provide Feedback