Axis Properties - Tag Dialog Box Overview (AXIS_CIP_DRIVE)

Use the Tag dialog box to specify tag options for the axis tag.
Parameters
Name
Enter a name for the tag.
Description
Enter a description for the tag.
This field is optional.
Type
Displays the type of tag.
This field is read-only with a default value of Base.
Alias For
Displays the alias for the tag.
This field displays if the tag type is Alias.
This field appears dimmed on this dialog box.
Data Type
Displays the data type of the tag.
AXIS_CIP_DRIVE displays in this field, which is the only valid value for this dialog box.
Scope
Displays the scope of the tag.
External Access
Displays access rights for the tag.
Manual Tune
Click this button to open the Manual Tune dialog box in which you perform the manual tune function and run the drive.
OK
Click this button to accept or apply your edits for any of the settings in the dialog box.
Cancel
Click this button to cancel your edits for any of the settings in the dialog box.
Apply
Click this button to accept or apply your edits for any of the settings in the dialog box.
Help
Click this button for help for the settings in the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.