Motor Analyzer page
Use the
Motor Analyzer
tool to identify the parameters for motors that have the Data Source
on the Motor
page set to Nameplate Datasheet
.
TIP:
To open the Motor Analyzer page:
- In the Controller Organizer, expand the Motion Groups folder, and double-click an axis.
- From the Axis Properties dialog box, in Categories, expand the Motor folder, and then selectAnalyzer.
The
Motor Analyzer
tab provides three tests:- Dynamic Motor Test
- Static Motor Test
- Calculate Model
The tests analyze motor parameters for rotary and linear induction motors and permanent magnet motors. The parameters that appear on the tests depend on the motor type selected on the
Motor
page.If the test executes successfully and you accept the test values, the values populate the
Model Parameters
attributes. The type of motor selected affects the specific test results returned.All controls on the
Motor Analyzer
page are inactive if these conditions exist:- The project is offline.
- The project is online, and the drive associated to the axis does not support Motor Test.
- The project is online,Motor TestisEnabled, andAxis Configurationis set toFeedback Only.
- The project is online,Motor TestisEnabled, theAxis Configurationis not set toFeedback Onlyand theMotor Typeis set toNot Specified.
TIP:
If the controller is taken offline while a Motor Analyzer is executing, the test results are cleared the next time the tab is online.
Provide Feedback