- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Velocity Loop page
Use the settings on
Velocity Loop
page in the Axis Properties
dialog box to configure the velocity loop related parameters. These are the parameters for the Velocity Loop
page.
TIP:
To open the Velocity Loop page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickVelocity Loop.
Parameter | Description |
Bandwidth | Enter a value to determine the proportional gain, Kvp, of the velocity loop that multiplies the Velocity Error signal. This value represents the unity gain bandwidth of the velocity loop. |
Integrator Bandwidth | Enter a value (Hz) that represents the bandwidth of the velocity integrator beyond which the integrator is ineffective. A value of 0 for this attribute disables the integrator. |
Integrator | Enable or disable the velocity integrator status. |
Acceleration Feedforward | Enter a percentage for the Acceleration Feedforward. This parameter multiplies the signal to form the Acceleration Feedforward Command that is applied to the acceleration loop summing junction. When 100%, Acceleration Feedforward applies the full Acceleration Fine Command signal to the output of the velocity loop. |
Error Tolerance | Enter a value for the velocity error tolerance in user defined velocity units. The value determines the absolute maximum Velocity Error value that is tolerated without causing an Excessive Velocity Error exception. |
Lock Tolerance | Enter a value for the velocity lock tolerance in user defined velocity units. If the signal entering the velocity limiter exceeds this velocity limit value, the device responds by clamping the velocity reference to this limit and setting the Velocity Limit status bit. |
Velocity Limit Positive | Enter a value for the positive velocity limit in user defined position units. If the signal entering the velocity limiter exceeds this value, the device responds by clamping the velocity reference to this limit and setting the Velocity Limit status bit. |
Velocity Limit Negative | Enter a value for the negative velocity limit in user defined position units. This value reduces or eliminates velocity overshoot by subtracting a portion of the velocity reference signal from the velocity error. |
Standstill Window | Enter a value for the velocity standstill window in user defined position units/s. The configured value establishes a window around zero speed. When the Velocity Feedback signal is within this window, the Velocity Standstill status bit is set. When Velocity Feedback signal falls outside this window, the Velocity Standstill status bit clears. |
Threshold | Enter a value for the velocity threshold in position units/s. This parameter defines a minimum absolute velocity. If the magnitude of the Velocity Feedback signal is less than this value, the Velocity Threshold status bit is set. If the axis is set for Frequency Control, the Velocity Feedback signal derives from the Velocity Reference signal. |
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.Tip: The Parameter List page may contain more attributes than the associated page. In some cases, attributes that display on the Parameter List page do not display on the associated page. |
Provide Feedback