Changing EtherNet/IP Mode dialog box
The
Changing EtherNet/IP Mode
dialog box confirms the pending change to the EtherNet/IP Mode for controllers that support dual configurable Ethernet ports. It appears before a project is downloaded to the controller.Read the warnings listed in the dialog box, then continue or cancel the EtherNet/IP Mode change. Canceling the change stops the download.
The
Errors
tab in the Output
window shows progress during the EtherNet/IP Mode change and subsequent polling for power up. It also reports any errors that occur and whether the download has been canceled. Provide Feedback