Controller Properties dialog box - Nonvolatile Memory tab settings
The settings on the
Nonvolatile Memory
tab in the Controller Properties
dialog box provide access to nonvolatile operations. Some settings are not available for all controller types.
The ability to change the settings on this tab can be controlled by
FactoryTalk Security
permissions.Parameters | Description |
Name | The name of the stored controller image that resides in nonvolatile memory. |
Type | The controller type for the image stored in nonvolatile memory. This controller type can be any type that supports nonvolatile memory. |
Revision | The firmware revision of the controller when the image in nonvolatile memory was stored. In order for the image in nonvolatile memory to be loaded back into controller memory, the firmware revision of that image must match the revision of the controller. |
Load Image | The condition under which the image stored in nonvolatile memory is loaded back to controller memory. |
Load Mode | The mode the controller enters upon loading from nonvolatile memory. |
Safety Application | The nonvolatile memory safety lock status (locked or unlocked). Safety Application is available only when online or connected to a controller with a removable memory card that contains a Safety controller application. The Safety Application value is cleared when communication is lost. |
Safety Signature | The nonvolatile memory safety Signature status (ID, Date, and Time). Tip:
Compact GuardLogix 5380 and GuardLogix 5580 controllersSafety Signature is available only when online or connected to a controller with a removable memory card that contains a Safety controller application. |
Opens the Safety Signature ID dialog box to view and copy the entire 32 byte ID for Compact GuardLogix 5380 and GuardLogix 5580 controllers.Compact GuardLogix 5380 or GuardLogix 5580 controller | |
Image Note | Descriptive information that you entered at the time the image was stored in nonvolatile memory. |
Stored | The workstation date and time when the image is stored in nonvolatile memory. |
Inhibit Automatic Firmware Update | Select to inhibit (disable) the Automatic Firmware Update feature. The parameter is also available via an SSV/GSV instruction. If you inhibit the feature via an SSV instruction, this check box is selected. If you enable the feature via an SSV instruction, this check box is cleared. The controller, before initiating the automatic update of modules, checks this parameter and proceeds only if the feature is enabled. The parameter is available both offline and online, and unavailable if the controller has redundancy enabled on the Redundancy tab in the Controller Properties dialog box. |
Load/Store | Opens the Nonvolatile Memory Load/Store dialog box to load or store a project in nonvolatile memory, and to enable Firmware Supervisor. The button is unavailable when:
|
Status Bar | Shows the reason the Load/Store button is unavailable. Only shows one status at a time. Possible status messages:
|
Provide Feedback