Dependent scaling factor attributes

You have modified a scaling factor attribute that affects other attributes. The current list of affected attributes includes:
  • Maximum Speed
  • Maximum Acceleration
  • Maximum Deceleration
  • System Bandwidth
  • Ramp Velocity – Positive
  • Ramp Velocity – Negative
  • Ramp Acceleration
  • Ramp Deceleration
  • Position Lock Tolerance
  • Position Error Tolerance
  • Velocity Loop Bandwidth
  • Velocity Integrator Bandwidth
  • Velocity Error Tolerance
  • Velocity Threshold
  • Velocity Lock Tolerance
  • Velocity Standstill Window
  • Velocity Limit – Positive
  • Velocity Limit – Negative
  • Acceleration Limit
  • Deceleration Limit
  • Feedback Unit Ratio
  • System Inertia
  • Torque Limit – Positive
  • Torque Limit – Negative
  • Torque Threshold
  • Rated Slip Speed
  • Stopping Torque
Select Yes to recalculate and apply all dependent attribute values.
Select No to only apply the calculated scaling factors.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.