View Equipment Phase Performance Details
Use the
Monitor
tab of the Equipment Phase Properties
dialog to view run-time information of the Equipment Sequence, including maximum and last scan times, the current sequence state, and any owners.Before you begin
- Make sure the controller is offline.
To monitor an Equipment Sequence:
- Right-click on an Equipment Phase and selectProperties, or by double-click an Equipment Phase in theController Organizer.
- Select theMonitortab.
- View theScan times.
- Max: Displays the maximum amount of scan time of the Equipment Phase, in milliseconds.
- Last: Displays the last scan time of the Equipment Phase, in milliseconds.If you want to reset theMaxandLastscan times, and restart the scan timer, selectReset Max.
- View theStateandSubstate.
- State: Displays the current state of the Equipment Sequence: IDLE, COMPLETE, STOPPED, ABORTED, HELD, RESETTING, STOPPING, RUNNING, ABORTING, HOLDING, and RESTARTING.
- Substate: Displays the current pause substate of the Equipment Sequence: <No Display>; Pausing; Paused; Pausing, Auto Pause; and Paused, Auto Pause.
- View theOwners.
- If you reset the scan times, selectApply, thenOK. Otherwise selectCancel.
Provide Feedback