Equipment Sequence Element toolbar

How do I access the Equipment Sequence Element toolbar?
Double-click the diagram icon in the
Controller Organizer
to open an equipment sequence diagram.
The
Equipment Sequence
Element
toolbar is available in the offline mode only. Use the buttons on the
Equipment Sequence
Element
toolbar to add steps, transitions, and branch structures to a sequence diagram.
Equipment Sequence Element Buttons
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.