Add a selective divergence
Use
to create a divergence for a selective branch. In a selective divergence, only one of multiple paths is executed--the path containing the transition that first evaluates as TRUE.
Add Selective Divergence

To add a selective divergence:
- On theEquipment SequenceElement toolbar, selectAdd Selective Divergence
.
- Connect the divergence to a preceding step.
- Add execution paths to the divergence:
- Add and connect a transition to the divergence to create a separate execution path.
- Repeat to create additional execution paths as needed.
- Add and connect additional steps and transitions to each execution path as needed.
- Verify each execution path ends with a transition.
Provide Feedback