Add a simultaneous divergence
Use
to create a branch where all linked steps execute simultaneously.
Add Simultaneous Divergence

To add a simultaneous divergence:
- On the Equipment Sequence Element toolbar, selectAdd Simultaneous Divergence
.
- Link the divergence to a preceding transition.
- Add execution paths to the divergence:
- Add and connect a step or a step and transition pair to the divergence to create a separate execution path.
- Repeat to create additional execution paths as needed.
- Add and connect additional steps and transitions to each execution path as needed.
- Verify each execution path ends with a step.TIP: Use a simultaneous convergence to merge the paths.
Provide Feedback