ControlLogix Firmware

ControlLogix Firmware

The
Equipment Sequence
program firmware implements all the code necessary to manage the use of
Equipment Phase
programs, shares data between a sequence program and one or more
Equipment Phase
programs, and coordinates execution of the
Equipment Phase
s.
When an
Equipment Sequence
or sequence element changes status or an operator interacts with the
Equipment Sequence
, the firmware generates an event. Once an event is generated, it is published for external applications to receive.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal