Transition display states

Transition display states show how the transition execution relates to the overall
Equipment Sequence
execution.
Transition Display State
Transition Color
Description
IDLE
GRAY
The transition is not actively executing.
ARMED
GREEN
The transition is actively evaluating its expression.
FIRING
GREEN
The transition expression has evaluated TRUE. The previous steps is STOPPED and the next steps is started.
STOPPED
BLUE
The transition has completed processing a STOP command and has stopped the transition's execution.
ABORTED
PURPLE
A
Equipment Sequence
transition in the ABORTED state has been disabled by an ABORT command and will not advance an
Equipment Sequence
chart.
HELD
YELLOW/BROWN
An
Equipment Sequence
transition in the HELD state has been halted by a HOLD command or HELD because of an
Equipment Sequence
failure and will not initiate or advance the
Equipment Sequence
transition firing process until issued a RESTART command. If the transition has been HELD due to an
Equipment Sequence
failure, the failure should be cleared before issuing a RESTART command.
HOLDING
YELLOW/BROWN
An
Equipment Sequence
transition in the HOLDING state is advancing the
Equipment Sequence
transition firing process. This transitional state is only visible until the scan processing the HOLD command has finished.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.