- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
I/O Module Specification and Configuration
In a Logix Designer application project, all I/O modules must be manually added to the project. There is no auto-configuration tool available. Most of the I/O modules are software-configurable.
When you configure an I/O module, you specify characteristics specific to that module. The Logix Designer application automatically adds the predefined tags for the module as controller-scoped tags.
The configuration information for the module depends on the module you select.
You can specify electronic keying to reduce the possibility that you use the wrong device in a control system. It compares the device defined in your project to the installed device. If keying fails, a fault occurs.
Provide Feedback